11/10/2005 5:38 PM | |
Posts: 102 Rating: (3) |
Hai All, SOmebody please suggest me how to export the *.db files to Microsoft Excell Regards Shamsher |
11/10/2005 6:03 PM | |
Joined: 9/13/2005 Last visit: 11/18/2019 Posts: 86 Rating: (10) |
Hello Shamsher, two options that allow a data export of WinCC V6 are described in following FAQ: http://support.automation.siemens.com/WW/view/de/19300688 |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
11/11/2005 10:23 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
In addition to the two options mentioned by Freddy, you can also use |
This contribution was helpful to1 thankful Users |
11/25/2005 3:23 PM | |
Posts: 1084 Rating: (72) |
Then to be complete; If I run my query's on the same machine as where I run WinCC on, withOUT the Connectivity pack. It is legal? with regards. |
11/25/2005 3:35 PM | |
Posts: 1084 Rating: (72) |
And when buying one CAL, without Connectivity Pack, and running the query's on the same machine as wincc? |
12/7/2005 1:59 PM | |
Joined: 12/5/2005 Last visit: 8/20/2024 Posts: 239 Rating: (9) |
E-mail from Support. /------------------------------------------------------------------------------------------------------------------/ Dear Mr. Santos, to your mail: I'll use the OLE DB Provider for make reports in a PC with WinCC installed. In this case is not necessary a "Client Access License", ok? -->Yes. Where I can find more documentations and manuals of WinCC OLEDB Provider. --> The description of the query-syntax and examples are in the documentation of the Connectivity Pack. If you do not have such a CD, you can download the documentation from our FTP-Server with the following link: ftp://ftp.siemens.de/outgoing/Connpack61.zip /------------------------------------------------------------------------------------------------------------------/ This e-mail was send in 29/06/2005. The link, now,is broken. Therefore if you use DTS, VB, VC++, ASP, Macro, Script in a PC with WinCC, it is legal. You could copy this data for a new database and create a new server/client system with a free database, but this is very poor. Duplicated data are terrible solutions. Anyway, I used the Connectivity Pack 6.1 and I love it. I only don't liked of the DateTime field don't has a millissecond in the recordset of AlarmView, but exists a millissecond field, so is possible to create a DateTime with millissecond. And the recordset of Tag Logging provide access to data of Fast Archive, Slow Archive, Compressed Archive. |
Last edited by: Marcio at: 12/7/2005 2:02 PMMárcio Santos |
|
11/10/2006 9:03 AM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating: (151)
|
People have already posted example scripts on this forum [:D] Just use the search box to find the posts. |
Follow us on