8/12/2018 10:29 PM | |
Posts: 1 Rating: (0) |
I have issues with a F-DQ module(6ES7526-2BF00-0AB0) that keep going defective. We have 5x of the same type module in the rack and it's only this one module that goes defective. Note that this module is in the last slot of the 5. After the module has gone defective we can disconnect and reinsert it to make it work again, for a timeframe of about 10min to 2days, where it again will get the "defective" error. We have attempted to replace this module with brand new module but the same error occurs. We have also attempted to increase the f-monitoring time from 150ms to 500ms. The module has the latest firmware version 1.0.2. The CPU has the latest firmware version 2.5.2. Do anyone have experience with the same issues? Attached zip file of 3 diagnostic buffers: - Module is defective - Safety program: Error in PROFIsafe communication with F-I/O - Safety program: F-I/O passivated AttachmentDiagnostics.zip (244 Downloads) |
Follow us on