5/2/2016 5:12 PM | |
Posts: 24 Rating: (1) |
hi dear friends is there anyone who tell me how i can run MM420 with S7-414 with profibus? i mean the example program thank you ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/3/2016 9:34:22 AMNew subject after splitting |
|
5/2/2016 6:28 PM | |
Joined: 11/21/2007 Last visit: 8/12/2024 Posts: 2325 Rating: (308) |
Hello Here you go .. MICROMASTER 4: Function block to operate on Profibus DP ( For Micromaster drive with firmware < V4.0. ) MICROMASTER 4 & SINAMICS G120: Function block (FC14) to control an MM4 via PROFIBUS DP SINAMICS G120, SIMATIC ET200S, MICROMASTER 4: Acyclic reading and writing parameters of the frequency inverters via PROFINET and PROFIBUS hope this helps Cheers Navnag |
Last edited by: Navnag at: 5/2/2016 7:16:41 PMNew FC link added There is no such thing as the last bug in a program |
|
Follow us on