8/30/2019 8:45 AM | |
Posts: 5 Rating: (0) |
Lost connection to Server, i use an iot 2040 with Example Image 2.40, written with WinDiskManager on an SD-Card. i installe contrib-s7 and contrib-ocpua with npm install in the path from documentation. i made a flow for communication with an S7-314c-2PN/DP i read an DB and writte Inputs. the programm runns few minuten on the iot and then came conection lost to server. The same Flow runs on my Laptop with node lot hours without error AttachmentTest 6 (lesen SPS1,SPS2,Übergeben, OPC unconfig).txt (92 Downloads) |
9/2/2019 9:03 AM | |
Posts: 5 Rating: (0) |
I keep getting the mistake. I use two PLCs An S7-314c-2PN / DP is connected to IOT2040 via a switch per Profinet The second S7-314C-2DP has an IBH link S7 ++ as S7-412 connected to the S7 via MPI. The attached Word document shows the configuration in NodeRed. The IP addresses are correct When I test the program on Node Red on my laptop, I have no problems
AttachmentFehler.docx (99 Downloads) |
Follow us on