2/7/2013 9:07 AM | |
Posts: 4 Rating: (0) |
Dear all MM4 Speed control using Encoder pulse I have a project to control speed of motor using encoder pulses. I’m using Micromaster 440 drive(6SE6440-20D27-5CA1), Encoder card (6SE6400-0EN00-0AA0) and 1000 R.P.M Encoder , I need to know, is it possible to do this project and is there any special parameter adjustments in drive. Please let me know about it and it useful for me I attached my project drawing here. I wetting for your valuable reply Thank you Ketawala AttachmentEncoder Dig2.pdf (294 Downloads) |
This contribution was helpful to1 thankful Users |
2/11/2013 6:30 AM | |
Posts: 4 Rating: (0) |
Dear Drive expert Pls Repaly my question,I watting for your valuable responce Thank you Ketawala |
7/14/2013 12:20 AM | |
Joined: 7/8/2009 Last visit: 7/26/2023 Posts: 1974 Rating: (477)
|
For speed control using Encoder, you need not do anything special Just follow basic comissioning, set encoder details in P400, P408 - set control mode to Close loop vector control (P1300 - 21) Have a look at following Manuals for more help MICROMASTER Encoder Module Parameter List: MICROMASTER 440 Operating Instructions: MICROMASTER 440 0,12 kW - 250 kW Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
7/16/2013 8:27 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating: (31) |
Hi vithani, I think ketawala want to know whether encoder o/p directly can be speed reference for drive. and it is not possible and you are giving reference for encoder fb VP |
Follow us on