3/10/2018 3:41 PM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685) |
Hello Raphaël; The Moby E system is quite old, and has been discontinued on Siemens' site since 2010. https://support.industry.siemens.com/cs/ww/en/view/44466959 However, there is still some information in Product Support you would find useful:
https://support.industry.siemens.com/cs/ww/en/view/7301006
https://support.industry.siemens.com/cs/ww/en/view/7396024 One important point you should take into account: The Moby E system can be used with S5 PLCs or S7-300 CPUs; for installation with a S7-400, it must be installed in a ET 200M rack, and connected to the PLC through Profibus-DP. See the attachment below. Hope this helps, Daniel Chartier |
3/11/2018 8:56 PM | |
Joined: 4/8/2014 Last visit: 9/19/2024 Posts: 16 Rating: (0) |
Hello Daniel; Thanks for your answer. Indeed I will connect the ASM 470 on ET 200 rack and the system to the CPU 400 through Profibus. The main concern now is the soiftware. I have understood that I will need this software (SOFTWARE/DOCUMENTATION FOR IDENT, DVD - 6GT2080-2AA20). but my problem is that I am not confident on it. can it work with PCS7? Then I am looking for a trial version to test before ordering it. Do you have any link? Tanks again. |
3/12/2018 3:12 PM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685) |
Hello Raphael; There are the only links I have found on the Product Support discussing RFID systems with PCS 7 (and your hardware is not considered).:
https://support.industry.siemens.com/cs/ww/en/view/29351305
https://support.industry.siemens.com/tf/ww/en/posts/rfid-on-pcs7/82726/?page=0&pageSize=10 I can only suggest you open a Support request and ask Siemens techs about your possible solutions. Please make sure you provide them with all the necessary information on your project, including the fact that it is PCS 7-based, and give them the version of PCS 7 you are working with. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/12/2018 3:14:16 PM |
|
Follow us on