7/4/2011 6:52 AM | |
Joined: 7/4/2011 Last visit: 1/30/2024 Posts: 4 Rating: (0) |
Further to interfacing, I am using MS Virtual PC 2007 to connect to Micromaster M420. The virtual PC is XP SP3, I have installed Starter on it, and is working OK. Settings for Virtual PC allow COM1 port to be the same as the Virtual PC. Have tried to use the Diagnostics in the PG/PC interface and no slave is detected. Am using the Siemens serial cable and kit directly into the computer's COM port (Dell D620).
Do I set the host the same parameters (9600) as Starter requires or something different. Is there a better test mechanism? The MM420 has the USS speed set to 9600 and the bus address is set at 0. Splitted from set the PG/PC interface - PC COM-Port (USS) - MM440. |
Last edited by: O_Moderator at: 7/6/2011 2:24 PMnew subject after splitting |
|
Follow us on