4/12/2017 1:06 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Which drives do you have in your plant? Do you have for the drives a add-on library, like "Drive ES" library or do you use standard APL channel blocks FbDrive or FbSwtMMS? |
SIMATIC PCS 7 - Overview |
|
11/25/2017 5:24 PM | |
Joined: 6/23/2008 Last visit: 4/22/2024 Posts: 1165 Rating: (279)
|
Hi Sydney, additionally to telegram 20 you need to configure the profisafe telegram 30 in the hardware configuration (Step7) at the drive. Also you need to configure it in the configuration of the drive (e.g. by software tool 'Starter'). Make sure that the 'F_Dest_Add' matches on both sides. In CFC you use the block F_CH_BO to write to the single bits of the profisafe telegram. In e.g., if you just need STO (safe torque off) it's the first bit in the profisafe telegram. See attachment for an example. Best regards... AttachmentF_Config_Sinamics.zip (309 Downloads) |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
This contribution was helpful to2 thankful Users |
11/26/2017 12:03 PM | |
Joined: 6/23/2008 Last visit: 4/22/2024 Posts: 1165 Rating: (279)
|
Hi Sydney, I think what you request is not possible (at least not as a complete fail safe program). I also wonder what should be the benefit of your solution... I guess you know this apllication example already...but this is also showing only the way I mentioned in my previous post. Best regards.... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
7/9/2019 9:28 AM | |
Posts: 5 Rating: (1) |
Mark1507 additionally to telegram 20 you need to configure the profisafe telegram 30 in the hardware configuration (Step7) at the drive. Also you need to configure it in the configuration of the drive (e.g. by software tool 'Starter'). Make sure that the 'F_Dest_Add' matches on both sides. In CFC you use the block F_CH_BO to write to the single bits of the profisafe telegram. In e.g., if you just need STO (safe torque off) it's the first bit in the profisafe telegram. See attachment for an example. Best regards... AttachmentF_Config_Sinamics.zip(46 Downloads) Hello, I have tried to make same setting as you have shown on pictures attached, but I have received error message : Module not configured or parameter VALUE not supplied (COnfigure a mofule for this driver in HW config and link it in SIMATIC manager with the driver via "Create module driver") It looks like that compiler doesnt recognize this inputs as failsafe or something. I dont know is there anything additional necessary to set on G120C drive and profisafe telegram, but I didnt saw any other option. If anyone have solution for this, I would highly appriciate... Thanks in advance! |
Last edited by: TIAtral at: 07/09/2019 15:07:32 |
|
7/12/2019 9:38 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello TIAtral, did you know the application example Integration of a SINAMICS G120 (F version) in SIMATIC PCS 7. This application has been created to provide users with an easy way to integrate a SINAMICS G120 frequency converter (failsafe version) into PCS 7 and to configure the PROFIBUS and PROFIsafe settings accordingly. With regards |
Follow us on