2/20/2019 6:19 PM | |
Posts: 2 Rating: (0) |
Hello! I want to set up a RF210R Reader with an RF180C RFID Module but the connection doesn't work. When i set the "Execute" Parameter of the Reset Block to TRUE the Error E7FE0800 keeps appearing (Time out during "INIT" after 60s according to "TC3WG"). PLC is a 1511C-1, Connection is PROFINET IO. Reader is connected on Port 2 of the RF180C I did set up the RFID Module with the Technology Object according to "https://support.industry.siemens.com/cs/document/109483371/rfid-basic-examples%3A-simatic-rf200-via-rf180c?dti=0&lc=en-WW" Attached are some configs of my project (in german) I read in some other posts that the adressing of HW_Connect and LADDR could be wrong, but i'm not sure. I'd be glad if someone could help me. Thanks alot AttachmentRFID Config.zip (316 Downloads) |
Follow us on