6/12/2015 12:49 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71) |
Hi, which version of TIA are you using? |
6/12/2015 2:49 PM | |
Joined: 10/1/2013 Last visit: 4/17/2024 Posts: 605 Rating: (71) |
Hi, sadly you cannot use this example project in TIA V13 SP1. You can only inspect the calls of the blocks in "Main" (OB1). Don't upgrade the project to look at the call environment. Never the less, if you use TIA V13 SP1 you will have to use the blocks included in TIA. You will find those blocks in the Instruction view at "Optional packages" > "SIMATIC Ident". The interfaces of the new blocks are very similar to the old ones from the MOBY DVD project. Just look at how they are called and create your own project. For further details of the blocks check the manual:
Hope this helps.... |
This contribution was helpful to1 thankful Users |
Follow us on