3/27/2016 3:01 PM | |
Joined: 5/30/2013 Last visit: 9/17/2024 Posts: 112 Rating: (37) |
Hi ToVerm. why don't use FC_33 S5TI_TIM convert S5T to TIME For start read this post: "SIMATIC Timers" versus "IEC Timers" . I prefer solution Handling Time of Day! . Another thanks hdhosseini for one of more magnificent posts.
zzVss |
Last edited by: zzVss at: 3/27/2016 3:03:29 PM |
|
This contribution was helpful to1 thankful Users |
3/29/2016 10:01 PM | |
Joined: 5/30/2013 Last visit: 9/17/2024 Posts: 112 Rating: (37) |
Hi ToVerm, if I correctly understood yours the problems you wont different between format time S5T#10ms (min)... S5T#2h46m30s0ms (max) and format in HEX. Correct? That is it not >SimaticBCDTimer' and 'SimaticTimer"<.. Second, this is conference Visualization, and if you wont answer for yours question go to the conference "Industrial software". Time in HEX format: The time base defines the interval at which the number of units of time is to be decremented by one unit when the timer runs. Time base 0 (bit 13 = 0, bit 12 = 0) = 10 ms The number of units of time must be specified as a BCD-coded number. The range from 1 to 999 is possible. For more information see: SIMATIC STEP 7 V5.5 Statement List (STL) for S7-300 and S7-400 Programming the page 194. Best regards zzVss |
Last edited by: zzVss at: 3/29/2016 11:59:46 PM |
|
This contribution was helpful to1 thankful Users |
3/31/2016 9:08 AM | |
Posts: 648 Rating: (95) |
Hello ToVerm, why do you not use the Date/Time format? See this cahpter in the manuel https://support.industry.siemens.com/cs/us/en/view/102754925/65765406091. With best regards rh1990 |
3/31/2016 9:34 AM | |
Posts: 223 Rating: (0) |
Because it's a timer, not a time. But I solved the problem :) |
3/31/2016 9:47 AM | |
Posts: 648 Rating: (95) |
Ok sry, i missunterstood your Problem. All right. |
Follow us on