7/11/2020 4:37 PM | |
Posts: 23 Rating: (0) |
Hello everyone. Can not find a solution with my problem, need a tip. I have PCS7 V9.0 SP2 Redundand server pair. Startup as a service under user (not admin) account not goes correctly - when I logins later to the system and checks connections status - the status window is blank (and no tags connection on graphic screens). If I restarts runtime manually under the same user account then it goes fine, no problems, connection established and appears in status window. I made a test with empty project - same behaviour, so it not a corrupted project. Servers are in domain, service start under domain user, added to "User", "Simatic HMI", "Simatic NET" groups. The difference between manual and service start is visible in Diag folder. In file CCDmRtServer.log during manual startup everything is ok:
But on startup as a service it fails:
AttachmentServerConnectionsProblem.pdf (59 Downloads) |
Last edited by: executer01 at: 07/11/2020 16:42:28Last edited by: executer01 at: 07/11/2020 16:45:43Last edited by: executer01 at: 07/11/2020 17:01:32Last edited by: executer01 at: 07/11/2020 17:13:01Last edited by: Jen_Moderator at: 07/13/2020 10:42:03Optimized link. |
|
7/13/2020 9:13 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello executer01, do you access with Remote Desktop to the WinCC-PC? see manual https://support.industry.siemens.com/cs/ww/en/view/109736216/85290451851 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
7/13/2020 2:00 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2145)
|
Hello executer01, then it looks like a wrong installation. You may use the SIMATIC Assessment Suite - Data Collector (SAS-DC) - https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Service Request, and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to1 thankful Users |
Follow us on