11/13/2019 3:46 PM | |
Joined: 3/25/2008 Last visit: 9/20/2024 Posts: 193 Rating: (8) |
hello, put into trace n set (K170), n act (K167), I act (K115), adjust speed contlollerr P225, P226
|
11/28/2019 5:23 AM | |
Posts: 95 Rating: (0) |
thanks sir |
11/28/2019 6:07 AM | |
Joined: 5/12/2006 Last visit: 9/20/2024 Posts: 22365 Rating: (3011) |
Hello, use another adapter. For Masterdrive the Aten UC232A should be work.
Christoph |
11/29/2019 5:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
What was fault in motor? Was armature rewinding or field rewinding carried out? Please discuss with vendor get fault data & repairs work information.
Please refer SIMOREG DC-MASTER 6RA70; software version 3.1 manual, chapter 7.5 Start up procedure, topic 8 execution of optimisation run. Please check how DC drive is controlled via CNC i.e. is it on Profibus or stand alone. If it is on bus you need to connect DI & run optimisation procedure.
OK. Does motor run in field weakning mode? What type of speed feedback is connected? tacho or encoder? Is it working OK. Please attach motor name plate details here.
OK. Have you checked DC motor armature commutator & brushes condition? Is it OK? Please check above points. |
11/30/2019 11:26 AM | |
Posts: 95 Rating: (0) |
dear sir, value is here,also attached pdf file of parameters. p100 115 p101 400 p102 5.6 p108 5000 p741 ratio 20/1000 80 value p83 1 other point said by you,i am working on it as you said. Attachment6s (1).pdf (479 Downloads) |
11/30/2019 12:12 PM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, P108 should be 4000 instead of 5000. The attached back up is old one or latest (after failuer of motor)? |
11/30/2019 12:56 PM | |
Posts: 95 Rating: (0) |
this back up is old.but i have changed only drive.parameter is same as before. |
12/1/2019 7:25 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
If possible please attach latest back up, will help to find fault history data. |
12/2/2019 6:23 AM | |
Posts: 95 Rating: (0) |
when i done optimastion p051-25,when I done it,fault come f050.now what to do?what is faulty ? parameter? drive? motor? |
12/2/2019 8:12 AM | |
Posts: 95 Rating: (0) |
dear sir, at terminal 103 and 104 ,voltage fluctuate 6,7,8. |
Follow us on