4/29/2020 5:18 PM | |
Posts: 5 Rating: (0) |
Good afternoon. DMG DMU 50 machine. We wrote earlier about our problem. https://support.industry.siemens.com/tf/ww/en/posts/when-starting-the-spindle-the-engine-makes-one-revolution-and-stops-in-error/235546?page=0&pageSize=10 We Checked the encoder with an oscilloscope, it works perfectly. The output signal from the encoder is sent to the intermediate electronic Board for converting the analog signal to digital and is transmitted to the controller via profibus Protocol. Q: can I connect to the connector (photo2) using a computer and diagnose the output signal from the encoder ? What software can I use to do this? We configured the encoder strictly according to the manufacturer's instructions, and received output signals of the required amplitude and offset relative to each other. But the errors on the DMU 50 still do not disappear, the only option that I see is that the intermediate Board for converting the signal is not working. And is it even possible to buy this electronic Board separately somewhere? |
4/29/2020 5:19 PM | |
Posts: 5 Rating: (0) |
|
4/30/2020 1:42 PM | |
Joined: 10/11/2006 Last visit: 4/23/2024 Posts: 5821 Rating: (789)
|
Hello, please contact for spare part your SIEMENS partner: https://www.automation.siemens.com/aspa_app/?cntryid=CA&comptcid=v&lang=en |
With best regards, |
|
Follow us on