11/30/2008 2:47 PM | |
Posts: 1 Rating: (0) |
Dear Mr,Mrs We are working on a Fast Load Shedding system. This system is proposed to prevent the probable problems of power generators in case of power failure at 400kV or 63kV lines by means of shedding some non critical loads as fast as possible. In this system reaction time should be less than 100 msec. Four different hardware configurations are existed as our alternatives. Note: Reaction time is the elapsed time between changing of an interrupt type input and fast relays activation for shedding the proposed loads.You can see hardware configurations and more information about its in attached filesWe would be glad if deliver answers of the following questions from your side:
AttachmentCONFIGURATION.zip (386 Downloads) |
Follow us on