2/18/2008 11:27 AM | |
Posts: 76 Rating: (16) |
Dear all , Here we will begin a series of ( Theory of operation of Electric drives (how does a drive work ? ) not How to use ?) . I will do my best to 1-introduce the materials in clear sentences . 2- reference all info said 3- avoid the complex mathematical eqn. as possible 4- focus on the main concepts I hope you will like it .I'll accept any modifications suggestoins of you. here we go . In order to talk about drives we should know thw concepts of 1- power electronics 2- machines . so first threads will be on them . Induction Motor :- The induction motor is by far the most widely used choice for development application in industry and in the tertiary sector. Being both rugged and reliable, it is also the preferred choice for the variable-speed drive applications. Low cost, high reliability, fairly high efficiency, coupled with its ease of manufacture, makes it readily available in most parts of the world. Figure 1.1 shows the typical constitution of a Squirrel-Cage Induction Motor, which is composed by three sets of stator windings arranged around the stator core. There are no electrical connections to the rotor, which means that there are no brushes, commutator or slip rings to maintain and replace.(fig1.1 is attached ) Large induction motor can also have a wound rotor - Wound- Rotor Induction Motor. As the name suggests, these motors feature insulated copper windings in the rotor similar to those in the stator. The rotor windings are fed with power using slip rings and brushes, and therefore this rotor is substantially more costly, presenting more maintenance problems than squirrel-cage rotors. This type of induction motor was used in industrial applications in which the starting current, torque, and speed need to be precisely controlled. In new applications squirrel cage motors are by far the most widely used solution. In the induction motor, a rotating magnetic field is created in the stator by AC currents carried in stator windings. A three-phase voltage supply applied to the stator windings results in the creation of a magnetic field that moves around the stator - a rotating magnetic field. The moving magnetic field induces currents in the rotor conductors, in turn creating the rotor magnetic field. Magnetic forces in the rotor tend to follow the stator magnetic field, creating a motor torque. The speed of an induction motor is determined by the frequency of the powersupply, the motor number of poles, and to a smaller extent by the motor load. The speed decreases a few percent (typically 1-3%) when the motor goes from no-load to full load operation. Driven directly from the mains supply, induction motors have essentially a constant speed. Therefore, to control the motor speed, without the use of external mechanical devices, it is necessary to control the power supply frequency. Many motor applications would benefit in terms of energy consumption and process improvement, if the motor speed was modulated as a function of the process requirements. Again to avoid math. eqn . we will mention the the ind. m/c char. curve directly (see fig1.2) The key issue in speed control in the squirrel cage induction motor is the freq. of source where the speed is varied according to ( V=120 *F / P) where v is the speed , F is the freq of source(our key issue ) and P is number of poles (cannot be controlled ) Electronic Variable Speed Drives can produce variable frequency, variable voltage waveforms. If these waveforms are applied to the stator windings there will be a shift of torque-speed curve, maintaining a constant pull-out torque, and the same slope of the linear operation region of the curve. In this way, the motor speed is going to be proportional to the applied frequency generated by the VSD. see fig 1.3 The general configuration of most VSDs. The three-phase, 50Hz alternated current (AC) supply is initially converted to direct current (DC), then filtered and finally, the DC/AC inverter converts the DC voltage to the variable voltage and variable frequency output applied to the motor. see fig1.4 The adjustment of the motor speed through the use of VSDs can lead to better process control, less wear in the mechanical equipment, less acoustical noise, and significant energy savings. However, VSDs can have some disadvantages such as electromagnetic interference (EMI) generation, current harmonics introduction into the supply and the possible reduction of efficiency and lifetime of old motors. I hope these info. may add to you and were not boring. Ref :- 'Electric Machinary fudamentals ' chapman 'Electric Machinary fudamentals ' robert macpherson and laramore ' induction notes ' Ewen Ritchie Attachment1 attachments.zip (1687 Downloads) |
This contribution was helpful to11 thankful Users |
3/19/2008 9:19 PM | |
Joined: 2/14/2007 Last visit: 9/17/2024 Posts: 4 Rating: (0) |
Abdelaal, Thank you, Abubahmed |
4/24/2008 10:08 PM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (42) |
Nice thread Its been a while I read the basics thanks! |
4/28/2008 7:45 AM | |
Posts: 2348 Rating: (264) |
Nice^) Can you make something similar for programming micromaster? When i faced getting started it take some time to understand basic functionality. |
5/1/2008 6:48 PM | |
Posts: 148 Rating: (11) |
Dear Sir, I have changed my views I am very happy to say that most of the people in my department also like your topics. May I request you to continue this. |
7/31/2008 1:25 PM | |
Posts: 53 Rating: (0) |
Good One!!! Really refreshed our minds with the basics |
9/12/2008 8:33 PM | |
Posts: 75 Rating: (13) |
Very good thread!! |
9/19/2008 1:37 AM | |
Posts: 1064 Rating: (72) |
Very nice thread . It's nice to get back to the basic once in a while . I look forward to read more of you information |
6/9/2009 5:54 AM | |
Posts: 272 Rating: (4) |
V good thread. |
9/6/2012 7:26 PM | |
Posts: 4 Rating: (0) |
NICEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEEE |
Follow us on