3/21/2012 11:23 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Hello, together we are working on this and try to reduce the "down"time of the forum. Best regards O_Moderator |
4/8/2012 9:51 AM | |
Posts: 8946 Rating: (999) |
This problem happens to me also very often. Since my start-up here in 2008, this is not an new problem. Many times, I send a message twice because of that. |
4/18/2012 7:59 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
OK I got it... It was adblock Plus... I got from solution from here Regards, Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
4/19/2012 2:37 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Hello , I experienced a really rare and strange phenomenon.While completing a post and uploading an attachment,I lost my log in status.It is rare but it is like a disaster to remember all sentences. There is some complains in the German conference. Problem mit dem Forum: Login geht verlorenBest regards, Hamid Hosseini |
4/19/2012 2:55 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hello, I also experienced a really rare and strange things, The Thanks & Rate Button in not dispaly for Some User Post, See the Screen Shot.... AttachmentSiemens.zip (411 Downloads) |
Ammy |
|
4/19/2012 3:06 PM | |||||
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Sometimes this part:
is reduced to
|
||||
B r g d s , |
|||||
4/19/2012 3:30 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
After missing stars scenarion here,this is new in attachment. Missing stars,"thanks" and buttons all together. Best regards, Hamid Hosseini Attachmentmissing objects.zip (410 Downloads) |
4/19/2012 3:31 PM | |||||
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
This is old problem and mostly its because of heavy load And if you are using IE 7 or 8 then compability button always helps and For Mozilla, we dont have any option other than Type web address again in addressbar..And thats why I mostly prefer Open in New Tab button to see any forum so that I dont loose that FORUM button to go back to main page Regards Devesh Vithani |
||||
Last edited by: Vithani at: 4/19/2012 3:50 PMI dont Like people driving Fast, thats the reason I overtake them ;) |
|||||
Follow us on