7/1/2019 7:32 AM | |
Joined: 9/20/2014 Last visit: 2/7/2023 Posts: 56 Rating: (20) |
Hi all I have one project According to attachment , when I use The SIMATIC manager V 5.5 SP 2 and The D7-SYS v7.0 don't have problem for connect to the FM458 (I can go to Test mode ) but When I installed SIMATIC manager V5.6 and The D7-SYS v7.0 cannot go to test mode , In The HW config online The FM458 not online . what is Problem? Thanks AttachmentFM458.pdf (474 Downloads) |
7/1/2019 7:52 AM | |
Joined: 8/25/2006 Last visit: 5/8/2024 Posts: 2203 Rating: (277)
|
Hello. D7-SYS V7.0 is not compatible with Step 7 V5.6. Let's begin with MS OS: Step 7 V5.6 compatible with Win7, Win10, Win Server 2008, 2012, 2016. D7-SYS V7.0 is released for Win200, Win XP and Win server 2003. There could be more problems. |
Last edited by: Jen_Moderator at: 07/01/2019 14:19:05Optimized link. |
|
7/1/2019 10:40 AM | |
Joined: 9/20/2014 Last visit: 2/7/2023 Posts: 56 Rating: (20) |
Hello yes,you're right , I installed Windows 7 64 bit ,I think I need to install D7-SYS V8.2 Thanks for your Help |
Follow us on