9/15/2018 2:23 AM | |
Joined: 2/12/2018 Last visit: 1/13/2021 Posts: 19 Rating: (0) |
Thanks for your response! We are encountering the following problem: We taught positions with the real KUKA robot and now wanted to run the exact same path in our MCD model, which obviously has the same dimensions as the real machine. The problem is, in the MCD model, the taught positions are not reachable. We were thinking that maybe the distances are not set correctly in the KinematikSIM config.xml? Are the distances for d in meters? I attached the chain_config as a txt file. When is the application example for KinematikSim planned to be available? Is there a preliminary version with some basic descriptions? Thank you! Attachmentchain_config.txt (860 Downloads) |
Follow us on