7/20/2017 7:38 AM | |
Joined: 7/10/2017 Last visit: 2/8/2024 Posts: 111 Rating: (2) |
Hi, I am too working on FC14 with Sinamics cu240b-2dp for a very basic application like Conveyor for ON/OFF, REVERSE and SLOW & FAST speeds. I was able to execute FC14 successfully for ON/OFF and REVERSE, However I want to set a fixed speed in DRIVE for Slow & Fast operation and use that bit in PLC. Could you please suggest me which bit should i use for that and Can I use same Control Word 1 for this parameter also.....(FIXED SPEED SETPOINT 1)..... Hope you understood my question.....Thanks... ------------------------------------------------------------------------------------------ |
Last edited by: MustafaRaza at: 7/20/2017 7:54:11 AMLast edited by: MustafaRaza at: 7/20/2017 7:54:38 AMLast edited by: Jen_Moderator at: 7/21/2017 1:04:04 PMNew subject after splitting |
|
Follow us on