12/12/2019 12:25 PM | |
Joined: 10/14/2013 Last visit: 3/27/2024 Posts: 3 Rating: (0) |
when attempting to change P918 with drive monitor via serial i get a error message " Code word missing " and the address does not change, what is needed to allow the parameter to update? if i try and change from the PMU i get two rows of dashed lines and still no address change. the drive is not faulted, and i get the same results if the profibus is connected or not. thanks in advance
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/13/2019 07:41:30New subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on