6/26/2010 10:13 PM | |
Posts: 3 Rating: (0) |
hello which parameter/parametersdo i have to set if i want to command(start ands stop) an asynchronous triphase motor (through RS232-RS485 connection) usingDriveMonitor version 5.2.1.0? or what do i have to send trough the serial bus in order to do this(start and stop the motor) if i use LabWindows/CVI . thanks. Splitted from MM 440 connect to PC. |
Last edited by: O_Moderator at: 6/28/2010 9:36 AMnew subject after splitting |
|
Follow us on