6/3/2011 10:24 AM | |
Posts: 291 Rating: (69) |
Hi Saravana, I appologize for that...calling you "she"! Sorry!! By the way ~
Hi Shar, You're right! I've just finished installation of WinCC V7.0 SP1 on a fresh-installed Windows 7 + Office 2007 platform. Now I see the real Windows 7 has bigger system tray icons & different style of "Path title" shown in file Explorer. Though the above has nothing to do with Saravana's problem, just for your information~ '----------------------------------------------------------------------------------------------------------------------------- My installation went smoothly with SQL Server till WinCC HMI RT/CS...& so on. But... While installing the sorts of "SmartTools", "Archive Tool" & "Configuration Tool". An error message popped up for each of tham saying the same message that: the tool can be installed to one of the following OS only - --Windows XP SP2 or higher --IDS_SUP_ALLOWED_OS_L2 '----------------------------------------------------------------------------------------------------------------------------- (as the attached) Needless to say, now ~ I have WinCC V7.0 installed in Windows 7, without Cofiguration Tool installed there B.R., Komi AttachmentWin7_Install_Err3.zip (273 Downloads) |
Last edited by: Komi at: 6/3/2011 10:38 AMattach the screenshots ( Failed in uploading for several times, so chose only one for uploading. ) |
|
2/12/2016 10:43 AM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Hello, have you first install Excel or WinCC? |
2/12/2016 10:57 AM | |
Posts: 79 Rating: (9) |
Hi, You don't need this tools since console management is 'Excel like'... Regards |
Follow us on