1/16/2018 8:40 AM | |
Joined: 7/9/2015 Last visit: 4/24/2024 Posts: 3812 Rating: (554) |
Hi, you will have to activate / configure the integrated PTO/PWM function of S7-200. Check technical data of you PLC if it supports PTO/PWM. Check the following FAQ: How can you measure the exact length of an upcoming pulse with an S7-200?Regards, Towome |
|
|
1/16/2018 9:04 AM | |
Posts: 2826 Rating: (684) |
Hello Towome. The link is not helpful -- it links to HSC related task. Hello narove. The user manual (System Manual S7-200) is very good; see this for explanations. The software has "instruction wizards" that help you with the configuration. There is doubt to which hardware and software you are using. The notes above is not for the "S7-200 Smart" but for the "S7-200" (original / classic). |
1/16/2018 12:54 PM | |
Joined: 9/18/2015 Last visit: 2/10/2024 Posts: 132 Rating: (0) |
hello #dp what i have understand that the CPU 224 smart has PTO output otherwise the basic one doesn't have |
Follow us on