1/17/2018 10:45 AM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (39)
|
Hello, Yes MR. Berghof is right. You need to publish the "WebClient.asp", because this is only the WebNavigator-Client . Regards |
Grundkurs/Systemkurs WinCC V7: |
|
1/31/2018 3:54 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71)
|
Hi Luis, please check the Administering the users for WebNavigator Client Especially, these points are important: 2. ... If system authorization "Web access - monitoring only" has been enabled, the user is only allowed to monitor the WinCC project when acting as WebNavigator Client. ... 4. In the properties of the user, activate the "WebNavigator" option. |
mfG / Best regards |
|
11/5/2018 12:12 PM | |
Joined: 8/12/2016 Last visit: 4/25/2024 Posts: 101 Rating: (3) |
I am facing the same problem. Did you solve it?? |
Follow us on