7/22/2018 3:52 PM | |
Joined: 5/21/2018 Last visit: 7/12/2021 Posts: 49 Rating: (1) |
Hello, I try to use PUT and GET instruction between 1200 and 200 CPUS. But I am getting an error. I try to find the cause, for the error but could not find any clue. I would like clarrify from experts whether it (GET and PUT) is compatible for these tow (1200 and 200) CPUS. Here with I attach you the snap shot as a pdf. Looking forward to hear your response. Thank you. With regards AttachmentCommunicationBetwen1200and200.pdf (34 Downloads) |
7/22/2018 4:50 PM | |
Posts: 2826 Rating: (684) |
1. Caution: The ET200 and S7-200 is not the same thing. 2. Which communication medium is used? RS232 / RS485 / Ethernet / Profibus /.. |
Follow us on