10/25/2018 12:50 PM | |
Joined: 10/11/2006 Last visit: 5/8/2024 Posts: 5836 Rating: (790)
|
Hello, that is the correct behavior, P115 changes back to 0 after the internal calculation was done. Please see the compendium in chapter 6.2 for the parameterizing steps and don't forget to do the power section definition as shown in chapter 6.2.1. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
10/30/2018 10:53 AM | |
Posts: 40 Rating: (0) |
ok thank u, but p115 return to 0 immediately and the motor did not move , i but p115 = 2 and after a while (20sec) it display f114 |
10/30/2018 10:54 AM | |
Posts: 40 Rating: (0) |
|
10/30/2018 10:55 AM | |
Posts: 40 Rating: (0) |
|
11/5/2018 10:25 AM | |
Posts: 40 Rating: (0) |
how can i perform auto parameterizing with p115=1 |
11/16/2018 7:51 AM | |
Joined: 1/16/2015 Last visit: 4/25/2024 Posts: 46 Rating: (1) |
Did you adjust P70 to match your converter? |
12/6/2018 11:21 AM | |
Posts: 40 Rating: (0) |
yes |
Follow us on