4/18/2019 5:19 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear All, These questions come to my mind. 1. How to measure the speed/ performance of the Terminal bus or System bus? 2. How could we know the network is healthy? Just like our CPU loading/performance in task manager, do we have a tool to test it out? |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
4/19/2019 8:40 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi JazTai, You have several tools available to measure performance: - WinCC Channel Diagnosis (via Start->Siemens Automation->SIMATIC->WinCC->Tools This tool shows information about the connections between OS and AS. You can see if there are errors, or if there is a buffer (Request queue size > 0). If there is a buffer, WinCC can become very slow. - Apdiag (Under Program Files(x86)->SIEMENS->WinCC->utools). This is a tool which returns script errors/print commands in scripts. It can give you a overview the scripting used in the system. - PC DiagMonitor (via Start->Siemens Automation->SIMATIC). This program is installed automatically on a IPC PC. It let's you monitor the condition of the IPC There are a lot more options to explore. Please check the following manual: PCS7 V9.0 Service and diagnostics In this manual, you can find a complete overview. |
Last edited by: Jen_Moderator at: 4/20/2019 11:35:14 AMOptimized link. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
4/23/2019 4:08 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Thank you so much for the manuals and suggestions. ( I learnt something from it) And I also found another way of monitor the loading of a window server station which is by using performance monitor. Not quite relevant to the network performance. I attached a screenshot on the performance monitor. I is a good way to monitor the system loading, which it allows us to build data collector set, monitor the system, and then record all the data and be ready to export out as CSV file for post analysis. |
Last edited by: JazTai at: 4/23/2019 4:21:33 PMLast edited by: JazTai at: 4/23/2019 4:21:52 PMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on