3/27/2017 10:22 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I encountered a issue with the error popped out dialog box "SFC chart does not exist (any longer). Note (1739:20). the error was occurred i done modification on some SFC types and instances. The project did not have these issues before. I was found when I finished my modification, intend to do compilation and download. The compilation did not have any problem. However during download and identifying the error, i found this error dialog box popped out. (pic attached) After that, i try to clean up my blocks database, check consistency, full compilation but could not work. then i tried to delete all the ES_MAP (block instance) , and do another full compilation and download, but the problem still occur the same, stuck at the download identifying step. Then i tried to delete all the chart , including sfc type, left only one simple chart, and do full compilation and download, but the problem still exist. After that, i did a save as with reorganization (slow) and try again, the issue still exist. Anyone got ideas on these? seem like siemens pcs 7 bugs to me. PCS 7 V8.2. |
Last edited by: JazTai at: 3/29/2017 8:10:49 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
3/27/2017 1:26 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello, you wrote, that it seems like a bug "Anyone got ideas on these? seem like siemens pcs 7 bugs to me." In such case, please contact the Technical Support. The simples way to do this, is to sending an Support Request via the following page: |
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to1 thankful Users |
3/28/2017 4:34 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Thanks for the reply. Yes, I have submitted a support request to Siemens. When i got the solution from siemens support, i will share it here again. In the meantime, if anyone know how to solve this issue, do share ya. |
Last edited by: JazTai at: 3/29/2017 8:11:32 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
3/29/2017 8:10 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Update, this problem had been resolved with CFC V8.2 Update 3. After install the update, I did a full compilation. after the full compilation, the project error ( SFC chart does not exist (any longer ), Error 1739:20 was resolved. Here attached with the pictures for your reference.
Just to update it here in case other engineers faced the same issues like me. To install the update, click the link below. Attached with CFC V8.2 update 3 Thanks. AttachmentSFC Chart Does Not Exist.zip (392 Downloads) |
Last edited by: JazTai at: 3/29/2017 8:12:14 AMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
3/30/2017 3:28 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Ya, Siemens solved that error code permanently with the CFC update 3. At least my problem was solved and i can continue my development. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
7/11/2019 4:17 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hello, you may check the update of your software here. Hope it helps. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on