6/19/2017 1:29 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
This Application Example describes how to collect data with the IOT2040 from an OPC UA Server and sending them to an IOT Hub in the Microsoft Azure Cloud. The example ends with the data being sent to the cloud. It is not included how to handle the data in the cloud or how to include them into an cloud application. That's user specific and described on the Microsoft Azure pages. The attachement includes a PDF file with the instructions and a folder to copy on the IOT. Best regards! AttachmentApplicationExample_OPC_UA_Azure.zip (2286 Downloads) |
Last edited by: bergmanu at: 6/23/2017 12:28:02 PMchanged attachement. Now whole .zip file not only the PDF Last edited by: bergmanu at: 7/3/2017 1:26:59 PMnow it's the fully application example.. including files and PDF Not working for IOT2050 support anymore from March 1st, 2024. |
|
7/3/2017 1:24 PM | |
Joined: 12/30/2016 Last visit: 2/15/2024 Posts: 1 Rating: (0) |
Hi, I'm very interested in this application but I don't find the attached pdf file Thank You |
11/23/2017 3:48 PM | |
Posts: 1 Rating: (0) |
Hi, I have a question. Do we really need SIMATIC IOT2000 in our applicaion? Can we omit it? Can we only use S7-1500 TIA Portal and Azure? Thank for your help!! |
11/24/2017 7:48 AM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, with the S7-1500 it is possible to get directly connected to the Microsoft Azure. There is an application example, which includes a MQTT function block for the S7-1500. I am not sure if you want to have your PLC directly connected to the internet.. If yes this should be possible. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on