9/20/2018 11:31 AM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
I also would like to use the 4G modem hardware from Telit which worked fine with an adjusted IOT2040 image which has been provided to me by Telit directly in the past. Now I have built an own customized SD image for a specific application case with the latest Siemens´ provided image version on GIT but I do not know what I would need further to add to it to make it possible that also the modem hardware from Telit will work. Also I discovered with the latest standard IOT2040 image version that there is something under iot2000setup in this context to set up the configuration and interfaces for cellular communication which unfortunately is not working out!!! Can you help me here please: - Is there still the need to build and add needed layers on top of my customized image? - Or how to solve the problem with the iot2000setup in this case as it is obviously not working out? ------------------------------------------------------------------------------------------ AttachmentScreenshots related to problem.pdf (111 Downloads) |
Last edited by: Jen_Moderator at: 9/21/2018 6:53:34 AMNew subject after splitting |
|
9/20/2018 5:25 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Have you taken a look at this tutorial? It contains an instruction to install the PPP Daemon, which you are probably still missing. Kind regards! |
9/20/2018 6:37 PM | |
Joined: 11/17/2016 Last visit: 1/26/2021 Posts: 11 Rating: (1) |
Dear bermanu, I have already addressed "deinok" (=the successful guy) at git because it is not working out in my case The problem is already that trying "./list-modems" gives me following as output: [ /telit_0 ] At the same time it is possible to use AT commands under ttyACM0 in a proper way but to establish a ppp0 via pppd procedure is something I haven´t worked out so far... And also it would be nice using oforno instead of pppd of course. By the way: how to activate the kernel modules mentioned by deinok which somehow refer more to the application case of usb modems like it seems or do I missunderstand something? I actually would like to use the mPCIe Telit modem, the Telit HE-910 D Therefore the procedure under iot2000setup does not work out as well AttachmentScreenshots related to problem.pdf (99 Downloads) |
9/24/2018 2:21 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, So from what I understood in this thread the Telit HE910-D seems to work fine (config over iot2000setup) but the HE910 does not work? Kind regards! |
Follow us on