10/2/2018 4:48 PM | |
Posts: 5 Rating: (0) |
Hi everyone, I have been trying to configure a Software PLC CPU1507S installed in a nanobox. The thing is that I can see the PLC in the avaible devices (PLC.PNG). The flash LED works. But when I go online there is a "Device Not compatible" in the slot of the PLC in the project tree (not_compatible.png). When I looked in the PLC specs in the nanobox, under the TIA PORTAL it is written V15 (PLC_NANO.png). I am currently using TIA PORTAL V14 to configure the station. Does this mean I should install TIA PORTAL V15 in order to make it work, or I am missing something in my configuration? I have added the project and the pngs in the attachment. Best Regards, Juan Norton AttachmentS1500_NANO.zip (256 Downloads) |
10/2/2018 4:50 PM | |
Posts: 5 Rating: (0) |
I have forgotten to add that the nanobox is an IPC227E |
Follow us on