3/13/2019 6:18 PM | |
Posts: 3 Rating: (0) |
Hello, Using TIA Portal v15 and Simotion Scout TIA V5.2 I have a Profinet-network with a D445, Absolute encoder and a CPX (valves). The encoder and CPX should work on IRT. The problem is the CPX has an update time of 4ms, while the domain setting of the D445 and encoder are 3ms. When I change the domain setting to 4ms I get the error that the Domain setting should be the same as the Integrated Profibus cycle time (3ms). Where and how can I change the Integrated Profibus cycle time? In TIA Portal when clicking on the Sinamics Integrated under Network View, going to Isochonous mode I can see the constant bus cycle time (3ms), but nothing I can change about it. See picture Sinamics PCI cycle. In the Simotion > Set system cycle clocks I cant change anything of relevance either. Picture System cycle clocks. No, the CPX cant be put on 3ms With the IRT Domain settings on 3ms and encoder on 3ms this works fine, but then the CPX cant be used on IRT. Added pictures as attachment. Thanks in advance! Attachment13032019.zip (194 Downloads) |
Last edited by: StafHJ at: 3/13/2019 6:20:38 PM |
|
Follow us on