(2)| 6/24/2015 10:04 AM | |
|
Posts: 2 Rating:
|
Dear Experts, I have a system of S7-412 5H redundant bundle with two IM153-2 HF remote stations for IO modules, an unmanaged switch and PAC4200 energy analyzers. I need to establish a redundant MODBUS/TCP communication with the PAC 4200 via the integrated PN ports of the CPUs and read some values of analyzers as MODBUS client. So far, I tried to use the function blocks and the OB’s of “SIMATIC_ModbusTCP_PN_CPU_Redundant_DEMO” project (6AV6676-6MB10-0AX0) in my station and parametrized the data blocks with the Modbus/TCP PN Red Wizard.The problem I encounter is that, connection is established but all of the busy, done and error indicators are false according to the variable table in the demo. Moreover, when i look at DB915, there is something wrong with the parameters of the internally called function TSEND and TRCV. The id’s are assigned as 0 and there is an id mismatch for the connections (8086).The datablocks and OB’s used in the project are given in the screenshots.
Can you give me any suggestions about this event? |
Follow us on