11/17/2018 9:22 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Can you show me a picture of the simatic manager when you press the View button? Can you also upload a picture of the Installed Software, you can find this under Siemens Automation in the Start menu of Windows. I will take a look at it. Thank you |
If I could help you, you can use the RATE button. Thank you. |
|
11/18/2018 6:31 AM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
Here is a PDF for the installed software.AttachmentInstalled 18112018.pdf (212 Downloads) |
11/18/2018 7:56 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Process Device plant view is shown when you have a PDM project. How did you install PCS7? Did you select all components individual or did you install the package install like PCS7 Engineering Station? I haven't seen this yet before, but it looks like it isn't a PCS7 project. When you right click on the multiproject and select properties, do you see if PCS7 project is chosen? What happens if you open the APL example project? Can you select Component view, plant view and process object view? I will cross check your installed software with mine..maybe some component is not installed. |
If I could help you, you can use the RATE button. Thank you. |
|
11/19/2018 8:03 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi Alexander, Ah ok that makes things clearer. When PCS7 is successfully installed, the PCS7 wizard will create the project and it is always labelled as PCS7 project and not Step7 by default. I would highly suggest to reinstall PCS7 because some things are now corrupted or missing because of your intervention. |
If I could help you, you can use the RATE button. Thank you. |
|
11/20/2018 9:22 AM | |
Joined: 4/13/2013 Last visit: 9/15/2021 Posts: 14 Rating: (1) |
Hi Oreca, Thank you very much for the assistance offered. the clean Install solved the problem. |
11/20/2018 10:19 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Great! Good luck on your project! |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on