3/17/2018 8:59 PM | |
Joined: 6/20/2010 Last visit: 4/24/2024 Posts: 86 Rating: (0) |
I just bougtht a new LOGO 8 6ED1052-1MD00-0BA8, I can not send a new program becouse ask to me the login; I put "LOGO" but always says wrong. I restored to factory, anyway always says "wrong pasword" I did not put any password. I think that it`s possible the firmware but I can not get the link or file to update my sowfware. I`ve another LOGO 8 6ED10521CC01-0BA8 and I have not any problem. I need your help. Thanks for all. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 3/19/2018 6:45:08 AMNew subject after splitting |
|
3/17/2018 9:36 PM | |
Joined: 6/20/2010 Last visit: 4/24/2024 Posts: 86 Rating: (0) |
When I use the file don not let to my computer read it. Here is a pictures or "old" version of Logo 8 and new one. --Deleted Link-- AttachmentFirmware Logo.zip (264 Downloads) |
Last edited by: Jen_Moderator at: 3/19/2018 7:22:38 AMDelted link and added file as an attachment. |
|
3/17/2018 9:55 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32878 Rating: (4064)
|
Hello my friend, I do not speak Spanish, so I do not know what the error messages mean. But what I can see is that you are trying to update the LSC. Better is the very latest LSC V8.2. You can download these here: Demo software , upgrades/updates, drivers After the download you have a file named "Setup.exe". Start this as an administrator. Edit: |
Last edited by: ixo65 at: 3/17/2018 10:00:52 PM |
|
Follow us on