10/14/2018 10:05 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (871) |
V90 low intertia shaft height 20,30,40 mm motor side connectors are same for all 3 sizes & details are as below. Motor power connector - 6FX2003-0LL12 Incremental encoder connector - 6FX2003-0SL12 Absolute encoder - 6FX2003-0DB12 For Brake - 6FX2003-0LL52 HTH |
10/16/2018 8:30 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (871) |
Please read the product details carefully. Motor power & brake connector size is 0.5-0.75 sq. mm 4pole & 2 pole respectively. Absolute encoder signal connector is D type 15 pole female, incremental encoder is 12 pole 0.2-0.25 sq. mm HTH. If you want dimentional details, then use this link. |
Last edited by: PISCEAN 2010 at: 10/16/2018 8:41:46 AM |
|
Follow us on