11/15/2016 8:01 PM | |
Posts: 30 Rating:
|
Hi 1) There are 100s if not 1000s of Arduino shields out there, can't recommend any off-hand, but this may help: http://playground.arduino.cc/Main/SimilarBoards#goShie and http://shieldlist.org/ 2) Yes 3) I too am curious about this, especially after reading the remark in the manual about not using a miniPCIe card that would overload the board. See section 7.4.3 in the manual (https://support.industry.siemens.com/cs/attachments/109741658/iot2000_operating_instructions_e_en-US.pdf?download=true ) 4) I don't know for sure, but it should. There doesn't appear to be an on/off button, so if power is removed and reapplied, it should power on. 5) Yes, the IOT2040 has a battery-backed real time clock (RTC) 6) If you are talking about an HMI/OIT to pair with this, best bet would be to connect through RS232, RS485, or Ethernet. There are also Arduino shields that have small LCD displays. Hope this helps. |
This contribution was helpful to
1 thankful Users |
4/12/2017 2:00 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by stoma is split to a separate thread with the subject Eclipse sample program. Best regards |
Follow us on