(0)| 12/12/2017 9:12 AM | |
|
Posts: 3 Rating:
|
Thanks for the guideline. I have only one question. I have tried to configure the management of alarms that, using the PLC and HMI acknowledgement, are aligned on two different HMI Panels at the same time. ( TP1200 / TP2200 ) I have tried also to use, for the trigger of several alarms, the same tag choosing different "Bit Triggering" and the same for PLC and HMI acknowledgement. What i found is that on the HMI acknowledgment tag ( ES: DB0.DBW0 ) if i choose for 3 alarms the bits 8, 10 and 12 ( ES: DB0.DBX0.0 , DB0.DBX0.2 and DB0.DBX0.4) when i acknolwedge one of those alarms all the bits regarding the "HMI acknowledgement TAG" are set ON. I make several tests and i see always the same event. That means that for different alarms i have to use different tags but is that really not possible use one tag for multiple alarms ? Sorry for the poor english and thanks in advance ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/12/2017 1:00:40 PMNew subject after splitting |
|
Follow us on