3/7/2018 8:30 AM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
"Updating" via Intel's repository is no longer recommendable (Intel stopped maintaining it long ago). Rather build your own fresh image according to https://github.com/siemens/meta-iot2000. |
3/23/2018 11:26 AM | |
Posts: 2 Rating: (1) |
Hello: That error (tar: unrecognized option '--strip-components=1') could be fixed by updating the Busybox package, since the developers added support for that option. This tutorial explains the steps to configure a full version from the GitHub repository: https://github.com/IntelOpenDesign/MakerNode/wiki/busybox:-configure-full-version I found the error with Intel Galileo and after updating the package the error did not appear, so I think it should also work with IOT2000. Anyway, for updating Node.js I agree that a fresh image is the right approach. Regards! |
This contribution was helpful to1 thankful Users |
Follow us on