6/21/2007 7:28 PM | |
Posts: 3149 Rating:
|
Hi if you bought ODK you should call the ODK-hotline ask there for an example. nemo |
6/22/2007 8:26 AM | |
Joined: 11/2/2006 Last visit: 5/29/2024 Posts: 15 Rating:
|
Hallo, I am just working on the same solution. Whit this working I got an example from ODK hotline, as you can see in the attached file. AttachmentODK TLGInsertArchivData.pdf (1442 Downloads) |
6/22/2007 9:42 AM | |
Posts: 133 Rating:
|
Thanks for your replay! And without ODK it is possible? For example using VB script: Connect to the SQL server and insert directly into the archive table? |
6/22/2007 10:41 AM | |
Posts: 14 Rating:
|
Thanks for solution. I put quick glance on that example, but i didn't test it yet. Generally it'd work, but i'm not sure about function "TLGInsertArchiveData" and structure "TLG_ARCHIVDATARAW". There're nothing like that in my ODK help (info for Nemo:I've already bought ODK V6.0 SP1 08/2003). May be there'll something in the new SP4 (new *.hor *.dll file). I'll get it on Monday and than i'll be much more clever For kukukk: I read that you have problem with "Substitute value" in WinCCin case of PLC disconnection (GPRS communication problem or something like that). So Mirco Sinaut SC is the OPC server and WinCC is a OPC client. Connection is lost with S7-200 station( GPRS modem), butconnection is alive between OPC server(Micro Sinaut SC) andWinCC and "Substittute value" won't be applied. You'd use "Station Configurator" and stop OPC server (Micro Sinaut). That's just guess. Please try and let me know. I'm still waiting for my Mirco Sinaut hardware. Simiens delivery system is soooo slow I think we shouldkeep in touch. My e-mail : peter.makyta@siemens.com. |
6/26/2007 11:33 AM | |
Posts: 1776 Rating:
|
Hi, maybe the FAQ is intersting for You http://support.automation.siemens.com/WW/view/de/22578952 April |
This contribution was helpful to
1 thankful Users |
Follow us on