1/10/2019 11:11 AM | |
Posts: 8 Rating: (0) |
Hello, I'm new in EnMPRO. I do not understand how I can make a loop in which two data points are summed up. I created a loop, put the input data points there, created the output data point, made a simple prototype, but the output data point is empty. How do I correctly sum the two data points? Version is EnMPRO V7.0 update 3 Best regards
AttachmentScreenshots.pdf (228 Downloads) |
Last edited by: Igorek536 at: 1/10/2019 11:25:36 AM |
|
1/11/2019 1:56 PM | |
Posts: 8 Rating: (0) |
Hello, datapoints and loop use the same process. Best regards |
1/14/2019 10:45 AM | |
Posts: 8 Rating: (0) |
Thanks for the answer. I set the kernel flag, restart the kernel, but nothing has changed.e_Result configuration in the attachment. Best regards |
1/14/2019 3:24 PM | |
Posts: 8 Rating: (0) |
I solved the problem myself.I forgot to set the flag "log to db" in e_Result. Best regards |
Follow us on