1/21/2019 9:56 PM | |
Joined: 12/11/2018 Last visit: 1/13/2021 Posts: 4 Rating: (0) |
Hello everyone, I would ask you for advice on wiring of the S0 input (Electricity meter) to Logo8 for Monitoring of Energy Consumption on Logos "fast" digital input. Hardware Logo8: (6ED 1052-1MD08-0BA0) Electricity meter: SDM 120DB MID (Link) Based on electricity meter wiring scheme (please find in above Link), there are two S0 Pulse outputs from Electricity meter (6+7), but only one Logo Input should be used. How should be an electricity meter wired to the Logo? Outputs 6+7 in single Logo Input, or is that an error? Many thanks for your support. Regards, GT PS. I searched all the instructions, but I did not find useful information. |
Last edited by: gt001 at: 1/21/2019 9:57:43 PM |
|
1/21/2019 10:47 PM | |
Joined: 12/11/2018 Last visit: 1/13/2021 Posts: 4 Rating: (0) |
Great, now it's clear to me. Thank you! Regards, GT |
Follow us on