(0)| 3/24/2015 10:18 AM | |
|
Posts: 3 Rating:
|
I am using 1214C DC/DC/DC In TIA Portal 11 SP2. Issue- If I Add A MoveVelocity or MoveRelative Motion Control Block after 2-MoveVelocity + 3MoveRelative Block,Then The Blcoks Execute Command Shows True But The Block Does Not Work Practically i.e. Servo Motor Is Not Rotating.But I Don't Get Any ErrorId In Output of The Block Is There Any Limitation of No. of Motion Control Blocks To Be Used?
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 3/25/2015 11:28:41 AMNew subject after splitting |
|
| 4/6/2015 6:10 PM | |
|
Posts: 3 Rating:
|
Yogesh, A simple search of the S7-1200 manual led me to section 9.3 (Motion Control) in which I found the picture attached below of the info you need. |
Follow us on