12/18/2017 4:55 PM | |
Joined: 7/30/2012 Last visit: 9/16/2024 Posts: 335 Rating: (12) |
Hello!!! Any Idea ??? |
12/19/2017 1:22 AM | |
Joined: 9/27/2006 Last visit: 9/21/2024 Posts: 12282 Rating: (2684) |
Hello KB; This application note describes software and hardware equivalents between the S7-300 and S7-1500, in terms of migration: The hardware equivalent of the FM 352 is the TM Timer module, described below, as shown in the table in attachment (from the proposed manual)é 6ES7552-1AA00-0AB0 S7-1500, TM TIMER DIDQ 16X24V SIMATIC S7-1500, TM Timer DIDQ 16x 24 V time-controlled digital inputs and outputs max. 8 DI, 16 DQ of which max. 16 with time stamp, Count, PWM, oversampling For more details on the TM Timer (and other technological modules of interest) examine the following document:
https://support.industry.siemens.com/cs/fr/en/view/59709820 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/19/2017 1:26:16 AMLast edited by: Jen_Moderator at: 12/19/2017 11:30:36 AMInserted right links. |
|
Follow us on