2/23/2018 3:47 PM | |
Posts: 241 Rating: (1) |
hello I mean in FC IN parameter the parameter with data type : TIMER |
2/24/2018 9:27 PM | |
Posts: 2826 Rating: (682) |
Hello CaOd.
What Hamed is referring to is passing on a timer (S5-Timer) through the parameter call of an FC. This a type of indirect addressing. Address passing. @Hamed - Sorry I do not have these informations with me and it has been too long for not working with the S7-300 series. All I can suggest is to for you to focus your search on method to indirectly work with (hardware) Timers and Counters. Most of us however built our own software timers and used those instead. It was a more clean way of doing timings and also had the added advantage of making retentive time counters when it was needed. Late note: If the timer is passed through with the parameter, the handling of that timer is not a problem. The code is using the global timer. You should not have a problem. |
Last edited by: #dP at: 2/24/2018 9:36:49 PMadd late note and stripped text from the discussion |
|
This contribution was helpful to4 thankful Users |
Follow us on