9/20/2018 7:24 AM | |
Joined: 10/7/2009 Last visit: 9/9/2024 Posts: 266 Rating: (92) |
Dear IndusElec, If your question is how to set the speed limit of G120C via PLC & HMI, you can do it in the user program using SINA_PARA_S (single parameter) or SINA_PARA (multiple parameters) of the Drive_Lib (same Global libraries folder as SINA_SPEED). Please refer to the attached documents. For G120C: parameters for the speed limitation p1082: Maximum speed (factory setting: 1500 rpm) p1083: Speed limit, positive direction of rotation (factory setting: 210,000 rpm) p1085: CI: Speed limit, positive direction of rotation (factory setting: 1083) p1086: Speed limit, negative direction of rotation (factory setting: -210,000 rpm) p1088: CI: Speed limit, negative direction of rotation (factory setting: 1086) Best regards, Yu-wen Attachmentsina_para.zip (51 Downloads) |
Last edited by: Yu-wen Tang at: 9/20/2018 7:38:59 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on