6/24/2019 10:37 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
The first way is to use different messages for start time and stop time, then you can use the activation date and time for the messages. If you want to display both on one display, then it is possible to synchronize a stopwatch with a week timer on 12:00 PM. The stopwatch then is used as a day timer and you can use several times in one message. On the first day the day time may have a wrong time until 12:00 PM. See attached file for example, Scorp AttachmentTimeStamp1.zip (108 Downloads) |
Last edited by: Scorp at: 06/24/2019 22:38:07 |
|
Follow us on