4/20/2020 9:50 AM | |
Joined: 3/29/2012 Last visit: 9/11/2024 Posts: 61 Rating: (0) |
Thanks for the prompt reply. The part number for three of the LOGO is 6ED10521fb00-0bA8 with Firmware verison V1.08.02. The fourth one has the part number of 6ED10521fb08-0BA0 with firmware version 1.82.02. Attached is the program as requested by you. please note that LOGO 3 Output 5 to Output 12 make use of shift register bits , Output 17 and Output 19 of the same LOGO 3B025 also make use of shift register bits. Output 1 and Output 2, Output 5 to Output 8, Output 9 to Output 12 of LOGO 4 also make use of shift register bits. B016, B034 and B049 are LOGO 4 shift register blocks. B025 and B070 are LOGO 3 shift register Block. Thanks AttachmentJOHNLUCK_HOME_PROJECT_LATEST_VERSION.zip (574 Downloads) |
johnluck |
|
4/21/2020 3:02 PM | |
Joined: 12/18/2014 Last visit: 9/23/2024 Posts: 33818 Rating: (4201)
|
I'm sorry, but I can't help you with that. Maybe Siemens can help you. Start a Support Request. |
4/21/2020 5:21 PM | |
Joined: 3/29/2012 Last visit: 9/11/2024 Posts: 61 Rating: (0) |
Okay thanks. I will do as you suggested.. |
johnluck |
|
7/31/2023 12:03 PM | |
Joined: 5/16/2022 Last visit: 10/8/2023 Posts: 6 Rating: (0) |
Thanks Johnluck, I am currently struggling to reproduce the issue on my test hardware which is running the latest firmware. I have been searching the Siemens website for the various firmware packages for the LOGO! and have only found the most recent one (1.83.02) and its changelog. I'm wondering if this is a firmware bug that has been sorted in an update, but unfortunately I didn't think to pull the firmware version from the site that is affected! [snip] ixo65...I've uploaded the essence of the program that is causing the problem. The shift register is initialised to have its first bit high and each pulse on I1 then steps the bit through the shift register. M1-10 in the real program are message texts, so the effect is that I1 scrolls through all the screens. What is happening is that on power cycling the unit in question comes back up with M1 and M2 active. It is almost as if B003 is set to be retentive (which it isn't). By setting it to retentive I can reproduce the behaviour exactly in both simulation and hardware AttachmentShift Register Bug Demo.zip (483 Downloads) |
Last edited by: Jen_Moderator at: 08/01/2023 07:54:46Division of question into separate topic. |
|
Follow us on