4/25/2020 10:05 AM | |
Posts: 5 Rating: (0) |
Hi, Just been reading the post and I need something similar, im using a current transducer to monitor motor current (0-10v), for arguments sake if the motor runs at 1A under normal circumstance is it possible to switch a memory bit or an output if the current was 1.25A? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2020 06:39:23New subject after splitting |
|
4/25/2020 10:35 AM | |
Joined: 12/18/2014 Last visit: 5/3/2024 Posts: 32954 Rating: (4073)
|
Here's a example for a current 0-20A.
AttachmentOverload_FS4.zip (66 Downloads) |
4/30/2020 11:59 PM | |
Posts: 5 Rating: (0) |
Hi, Thanks for responding but I can't seem to open the zip file, What program should it open in? |
Follow us on